The results of the assembly are output to the assemble list file.
Select the build tool node on the project tree and select the [Compile Options] tab on the Property panel.
To output the assemble list, select [Yes (-listfile)] on the [Outputs a source list file] property in the [List] category.

Select the build tool node on the project tree and select the [Assemble Options] tab on the Property panel.
To output the assemble list, select [Yes (-listfile)] on the [Outputs an assemble list file] property in the [List] category.