Select the build tool node on the project tree and select the [Compile Options] tab on the Property panel.
The macro definition setting is made with the [Define Preprocessor Symbol] property in the [Preprocess] category.

If you click the [...] button, the Text Edit dialog box will open.

Enter the macro definition in [Text] in the format of "macro name=defined value", with one macro name per line.
You can specify up to 256 characters per line, up to 256 lines.
The "=defined value" part can be omitted, and in this case, "1" is used as the defined value.
If you click the [OK] button, the entered macro definitions are displayed as subproperties.

To change the macro definitions, you can use the [...] button or enter the path directly in the text box of the subproperty.
You can also set the option in the same way with the [Define Preprocessor Symbol] property in the [Frequently Used Options(for Compile)] category on the [Common Options] tab. |