The output formats of messages are as follows.
- | When the file name and line number are included |
- | Message number type is information |
|
file-name (line-number):message-number:[information-type] message
|
The information type is change, insertion, deletion, or information.
- | Message number type is other than information |
|
file-name (line-number):message-number:message
|
- | When the file name and line number are not included |
The message number is output as a consecutive string consisting of one alphabetic character, 0592, and a three-digit number.