Configures the analog voltage input pin for A/D conversion.
Remark The value specified in argument channel is set to analog input channel specification register (ADS).
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_adc.h”
MD_STATUS R_ADC_Set_ADChannel ( ad_channel_t channel );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       ad_channel_t channel;  | 
    
       Analog voltage input pin ADCHANNELn: Input pin  | 
Remark See the header file r_cg_adc.h for details about the analog voltage input pin ADCHANNELn.
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument specification  |