Operates the unsigned multiply-accumulate.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_mac32bit.h”
void R_MAC32Bit_MACUnsigned ( uint32_t data_a, uint32_t data_b, mac32bit_uint64_t
* buffer_64bit );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint32_t data_a;  | 
    
       Multiplicand  | 
| 
       I  | 
    
       uint32_t data_b;  | 
    
       Multiplier  | 
| 
       O  | 
    
       mac32bit_uint64_t * buffer_64bit;  | 
    
       Accumulation initial value / Multiplier result  | 
Remark See R_MAC32Bit_MULUnsigned for details about the mac32bit_uint64_t.
None.