R_TMR_KBm_ForcedOutput_mn_Stop
 
Disables input of the trigger signal 
used for the forced output stop function.
 
[Syntax]
void   
R_TMR_KBm_ForcedOutput_mn_Stop ( void );
 
Remark         
m is the unit number, and n is the channel number.
 
[Argument(s)]
None.
 
[Return 
value]
None.