Performs processing in response to the LIN-UART reception status interrupt INTLS.
Remark This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS.
[Syntax]
static void r_uartfn_callback_error ( uint8_t err_type );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint8_t err_type;  | 
    
       Trigger for LIN-UART reception status interrupt 00000xx1B: Overrun error 00000x1xB: Parity error 000001xxB: Framing error  | 
[Return value]
None.