Usage example
Use timer as One-shot timer.
[GUI setting example]
| 
       12 bit interval timer  | 
    
       Used  | |||
| 
       IT  | 
    
       Used  | |||
| 
       Interval timer operation setting  | 
    
       Used  | |||
| 
       Interval value  | 
    
       100ms (Actual value:100)  | |||
| 
       Detection of interval signal (INTIT)  | 
    
       Used  | |||
| 
       Priority  | 
    
       Low  | |||
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start IT module operation */
R_IT_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_it_user.c
static void __near r_it_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop IT module operation */
R_IT_Stop();
/* End user code. Do not edit comment generated here */
}