Everything

Usage example

Use timer as One-shot timer.

 

[GUI setting example]

8bit interval timer

Used

IT8bit0

Used

Channel0

Used

Channel 0

8 bit

Interval timer operation setting

Auto

Interval value

100ms (Actual value:7.8125)

Detection of compare match (INTIT00)

Used

Priority

Low

 

[API setting example]

r_cg_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Start 8 bit interval timer unit0 Channel0 operation */

       R_IT8Bit0_Channel0_Start();

 

       while (1U)

       {

              ;

       }

       /* End user code. Do not edit comment generated here */

}

 

r_cg_it8bit_user.c

static void __near r_it8bit0_channel0_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       /* Stop 8 bit interval timer unit0 Channel0 operation */

       R_IT8Bit0_Channel0_Stop();

       /* End user code. Do not edit comment generated here */

}