Usage example
Use timer as One-shot timer.
[GUI setting example]
| 
       Timer  | 
    
       Used  | |||
| 
       TAU0  | 
    
       Unused  | |||
| 
       WUTM  | 
    
       Used  | |||
| 
       16-bit wake-up timer operation setting  | 
    
       Used  | |||
| 
       Count clock setting  | 
    
       Auto  | |||
| 
       Interval value  | 
    
       100ms (Actual value:100)  | |||
| 
       WUTM and WUTMCMP match, generate an interrupt (INTWUTM)  | 
    
       Used  | |||
| 
       Priority(INTWUTM)  | 
    
       Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start WUTM counter */
R_WUTM_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_timer_user.c
static void __near r_wutm_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop WUTM counter */
R_WUTM_Stop();
/* End user code. Do not edit comment generated here */
}