Everything

Usage example (Output compare mode)

Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.

 

[Waveform example]

 

[GUI setting example]

TimerRG

Used

TMRG

Used

Functions

Output compare function

Count source setting

Internal clock

Internal clock setting

Auto

TRG counter setting (Counter clear)

Clear by TRGGRA compare match

Register function setting (TRGGRC)

General register

Register function setting (TRGGRD)

General register

Compare value setting (TRGGRA)

100μs (Actual value:100)

Output setting (TRGIOA pin)

Toggle output

Enable TRGGRA compare match interrupt

Used

Enable TRGoverflowinterrupt

Unused

INTTRG priority

Low/ level3(low priority level)

 

 

[API setting example]

r_cg_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Start the TMRG module operation */

       R_TMRG0_Start();

 

       while (1U)

       {

              ;

       }

       /* End user code. Do not edit comment generated here */

}