Usage example (Slave, Reception)
Receive 4Bytes data by Slave.
[GUI setting example]
| 
       Serial  | 
    
       Used  | |||
| 
       SAU0  | 
    
       Unused  | |||
| 
       SAU1  | 
    
       Unused  | |||
| 
       IICA0  | 
    
       Used  | |||
| 
       Transfer mode  | 
    
       Slave  | |||
| 
       Slave0  | 
    ||||
| 
       Clock mode setting  | 
    
       fCLK/2  | |||
| 
       Local address setting  | 
    
       0xA0  | |||
| 
       Operation mode setting  | 
    
       Normal  | |||
| 
       Wakeup function setting  | 
    
       Off  | |||
| 
       Communication endinterrupt priority (INTIICA0)  | 
    
       Low  | |||
| 
       Slave transmission end (Callback function setting)  | 
    
       Unused  | |||
| 
       Slave reception end (Callback function setting)  | 
    
       Used  | |||
| 
       Slave error (Callback function setting)  | 
    
       Unused  | |||
[API setting example]
r_main.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_iica0_rx_buf[4];
/* End user code. Do not edit comment generated here */
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Receive data as slave mode */
R_IICA0_Slave_Receive((uint8_t *)g_iica0_rx_buf, 4U);
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_serial_user.c
static void r_iica0_callback_slave_receiveend(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop IICA0 module operation */
R_IICA0_Stop();
/* End user code. Do not edit comment generated here */
}