Usage example (Square wave output)
Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.
[Waveform example]

[GUI setting example]
| 
       Timer  | 
    
       Used  | |||
| 
       TAU0  | 
    
       Used  | |||
| 
       Channel0  | 
    ||||
| 
       channel 0  | 
    
       Square wave output  | |||
| 
       Square width  | 
    
       100μs (Actual value:100)  | |||
| 
       Generates INTTM00 and inverts timer output when counting is started  | 
    
       Unused  | |||
| 
       Initial output value  | 
    
       0  | |||
| 
       End of timer channel0 count, generate an interrupt (INTTM00)  | 
    
       Used  | |||
| 
       Priority (INTTM00)  | 
    
       Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TAU0 channel 0 counter */
R_TAU0_Channel0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}