This chapter describes the key functions provided by the Code Generator along with operation procedures.
Remark
In this chapter, an example where an RL78/L13 (ROM: 128KB) R5F10/WMG (80pin) is the target device is used to explain the key functions.