-
Main window
-
This is the first window to be open when CubeSuite+ is launched.
This window is used to control the user program execution and open panels for the build process.
This window can be opened as follows:
- Select Windows [start] -> [All programs] -> [Renesas Electronics CubeSuite+] -> [CubeSuite+]
Displays the menus relate to realtime OS.
Contents of each menu can be customized in the User Setting dialog box.
|
The [View] menu shows the cascading menu to start the tools of realtime OS.
|
|
|
Opens the Realtime OS Resource Information panel.
Note that this menu is disabled when the debug tool is not connected.
|
Displays the buttons relate to realtime OS.
Buttons on the toolbar can be customized in the User Setting dialog box. You can also create a new toolbar in the same dialog box.
|
Opens the Realtime OS Resource Information panel.
Note that this button is disabled when the debug tool is not connected.
|
The following panels are displayed in this area.
See the each panel section for details of the contents of the display.
Note See "CubeSuite+ RX Build" for details about the Output panel.