Everything

del_cyc

Outline
Delete cyclic handler.
C format
 ER      del_cyc (ID cycid);
Parameter(s)
I/O
Parameter
Description
I
 ID      cycid;
ID number of the cyclic handler.

Explanation
This service call can be called from tasks that belong to Trusted Domain.
This service call deletes the cyclic handler indicated by cycid.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- cycid < 0
- cycid > VTMAX_CYH
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_OACV
-27
Object access violation.
- The invoking task does not belong to trusted domain.
E_NOEXS
-42
Non-existent object.
- The cyclic handler specified by cycid does not exist.