Everything

del_dtq

Outline
Delete data queue.
C format
 ER      del_dtq (ID dtqid);
Parameter(s)
I/O
Parameter
Description
I
 ID      dtqid;
ID number of the data queue.

Explanation
This service call can be called from tasks that belong to Trusted Domain.
This service call deletes the data queue indicated by dtqid.
When there are waiting tasks for the target data queue by using snd_dtq, tsnd_dtq, rcv_dtq or trcv_dtq, this service call cancels the WAITING state of the tasks and returns E_DLT as a return value of the snd_dtq, tsnd_dtq, rcv_dtq or trcv_dtq.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- dtqid < 0
- dtqid > VTMAX_DTQ
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_OACV
-27
Object access violation.
- The invoking task does not belong to trusted domain.
E_NOEXS
-42
Non-existent object.
- The data queue specified by dtqid does not exist.