Everything

trcv_mbf

Outline
Receive from message buffer (with time-out).
C format
 ER_UINT  trcv_mbf (ID mbfid, VP msg, TMO tmout);
Parameter(s)
I/O
Parameter
Description
I
 ID      mbfid;
ID number of the message buffer.
O
 VP      msg;
Pointer to store the message.
I
 TMO     tmout;
Specified time-out (in millisecond).
TMO_FEVR: Waiting forever.
TMO_POL: Polling.
Value: Specified time-out.

Explanation
This service call processes as follows according to the situation of the message buffer specified by the parameter mbfid.
- There is a message in the message buffer.
This service call takes out the oldest message from the message buffer and stores the message to the area specified by msg and return the size of the message. As a result, the size of available space in the target message buffer increases by the amount calculated by the following expression.
The amount of increase = up4( Return value ) + VTSZ_MBFTBL
In addition, this service call repeats the following processing until task in the transmission wait queue is lost or it becomes impossible to store the message in the message buffer.
- When there is a task in the transmission wait queue and there is available space in the message buffer for the message specified by the task in the top of the transmission wait queue, the task is unlinked from the transmission wait queue and moves from the WAITING state (message transmission wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state. As a result, the size of available space in the target message buffer decreases by the amount calculated by the following expression.
The amount of decrease =up4( The message size sent by the task ) + VTSZ_MBFTBL
- There is no message in the message buffer and there is a task in the transmission wait queue.
This service call stores the message specified by the task in the top of the transmission wait queue to the area pointed by the parameter msg. As a result, the task is unlinked from the transmission wait queue and moves from the WAITING state (message transmission wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
Note, this situation is caused only when the size of the message buffer is 0.
- There is no message in the message buffer and there is no task in the transmission wait queue.
This service call queues the invoking task to the reception wait queue of the target message buffer and moves it from the RUNNING state to the WAITING state with time (message reception wait state).
The receiving WAITING state for a message buffer is cancelled in the following cases.
Receiving WAITING State for a Message Buffer Cancel Operation
Return Value
Message was sent to the message buffer area as a result of issuing snd_mbf.
E_OK
Message was sent to the message buffer area as a result of issuing psnd_mbf.
E_OK
Message was sent to the message buffer area as a result of issuing ipsnd_mbf.
E_OK
Message was sent to the message buffer area as a result of issuing tsnd_mbf.
E_OK
Forced release from waiting (accept rel_wai while waiting).
E_RLWAI
Forced release from waiting (accept irel_wai while waiting).
E_RLWAI
The time specified by tmout has elapsed.
E_TMOUT
Forced release from waiting (accept del_mbf while waiting).
E_DLT

Note 1 The maximum message size is defined at creating the message buffer. The size of the area pointed by msg must be not less than the maximum message size.
Note 2 Invoking tasks are queued to the reception wait queue of the target message buffer in the order of the message reception request.
Note 3 TMO_FEVR is specified for wait time tmout, processing equivalent to rcv_mbf will be executed. When TMO_POL is specified, processing equivalent to prcv_mbf will be executed.
Return value
Macro
Value
Description
-
Positive value
Normal completion (the size of the received message).
E_PAR
-17
Parameter error.
- msg == NULL
- tmout < -1
- tmout > (0x7FFFFFFF - TIC_NUME) / TIC_DENO
E_ID
-18
Invalid ID number.
- mbfid < 0
- mbfid > VTMAX_MBF
E_CTX
-25
Context error.
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
- The operand-write access to the area indicated by msg (start : msg, size : maximum message size specified at creation) has not been permitted to the invoking task.
E_NOEXS
-42
Non-existent object.
- The message buffer specified by mbfid does not exist.
E_RLWAI
-49
Forced release from the WAITING state.
- Accept rel_wai/irel_wai while waiting.
E_TMOUT
-50
Polling failure or specified time has elapsed.
E_DLT
-51
Waiting object deleted.
- Accept del_mbf while waiting.