Everything

[ RI600V4 ] tab

Outline
This tab shows the detailed information on RI600V4 to be used categorized by the following.
- Version Information
Display image
Explanation of each area
1 ) [Version Information]
The detailed information on the version of the RI600V4 are displayed.
Kernel version
Display the version of RI600V4 to be used.
Default
The version of the installed RI600V4
How to change
Changes not allowed
Install folder
Display the folder in which RI600V4 to be used is installed with the absolute path.
Default
The folder in which RI600V4 to be used is installed
How to change
Changes not allowed
Endian
Display the endian set in the project.
Display the same value as the value of the [Select endian] property of the build tool.
Default
The endian in the property of the build tool
How to change
Changes not allowed