-
[RI78V4] tab
-
This tab shows the detailed information on the RI78V4 to be used categorized by the following.
1 ) [Version Information]
The detailed information on the version of the RI78V4 are displayed.
|
Display the version of the RI78V4 to be used.
Note that the version is set permanently when the project is created, and cannot be changed.
|
|
|
|
|
|
Display the folder in which the RI78V4 to be used is installed with the absolute path.
|
|
The folder in which the RI78V4 to be used is installed
|
|
|
|
Display the memory model set in the project.
Display the same value as the value of the [Memory model type] property of the build tool.
|
|
The memory model selected in the property of the build tool
|
|
|