Everything

ref_ver

Outline
Reference version information.
C format
 ER      ref_ver ( T_RVER *pk_rver );

Assembly format
 MOVW    AX, #LOWW(_pk_rver)
 CALL    !!_ref_ver

Parameter(s)
I/O
Parameter
Description
O
 T_RVER  *pk_rver;
Pointer to the packet returning the version information.

Explanation
The service call stores version information packet (such as kernel maker's code) to the area specified by parameter pk_rver.
Note For details about the version information packet, refer to "12.5.9 Version information packet".
Return value
Macro
Value
Description
E_OK
0
Normal completion.