Everything

sns_ctx

Outline
Reference contexts.
C format
 BOOL    sns_ctx ( void );

Assembly format
 CALL    !!_sns_ctx

Parameter(s)
None.
Explanation
This service call acquires the context type of the processing program that issued this service call (non-task context or task context).
When this service call is terminated normally, the acquired context type (TRUE: non-task context, FALSE: task context) is returned.
Non-task contexts: cyclic handler, interrupt handler
Task contexts: task
Return value
Macro
Value
Description
TRUE
1
Normal completion (Non-task contexts).
FALSE
0
Normal completion (Task contexts).