-   
   vsta_sch
  
    -   
  
 Forced scheduler activation.
 
 ER      vsta_sch (void);
 This service call explicitly forces the RI850V4 scheduler to activate. If a scheduling request has been kept pending, task switching may therefore occur.
 
 Note	 The RI850V4 provides this service call as a function to activate a scheduler from a task for which preempt acknowledge status disable is defined during configuration.
 
 
  
  
    |  |  |  | 
  
    |  |  |  | 
  
    |  |  | 
 -	 This service call was issued from a non-task.
 
 -	 This service call was issued in the CPU locked state.
 
 -	 This service call was issued in the dispatching disabled state.
 |