Everything
1.6 Free Evaluation Editions

The free evaluation editions have a trial period of 60 days from the day of the first building by the compiler over which you can use features equivalent to those of the Professional editions.

After that period, the additional features of the Professional editions are no longer available, and the following restrictions apply:

-

[V2.07 or earlier] The total sizes of sections that can be allocated to the ROM area is up to 256 Kbytes. A linker error occurs if the size exceeds 256 Kbytes.

-

[V2.08 or later] The available optimization levels are -Onothing and -Odefault only. There are no restrictions on the section size.

 

The version number of the optimizing linkage editor is prefixed by W while a compiler is operating as an evaluation edition and by V when it is operating as a paid edition.

Examples are given below.

-

Version of a free evaluation edition:

Renesas Optimizing Linker W1.01.01 [25 Apr 2014]

-

Version of a paid edition:

Renesas Optimizing Linker V1.01.01 [25 Apr 2014]

 

We do not supply the following services for the evaluation editions. Consider purchasing a paid edition as necessary.

-

Technical support

-

E-mail delivery of items such as information on revisions