|
-SEction_forbid [V2.01.00 or later]
|
This option suppresses link-time optimization of specific sections.
[Specification format]
-SEction_forbid=sub [, ...]
sub:= ( section-name[, ...] )
| file ( section-name[, ...] )
| module ( section-name[, ...] )
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option suppresses link-time optimization of specific sections. |
- | Specify a section for which you wish to suppress link-time optimization with section-name. |
- | Specifying file or module prior to section-name allows link-time optimization to be suppressed for sections included in a specific input file or library module. |
- | Specify the input file name exactly as it is shown in the link map file, with uppercase and lowercase characters distinguished. |
[Output example of link map file]
*** Options ***
-Input=DefaultBuild\main.obj
|
- | If this option is specified more than once, all specifications will be valid. |
- | An error will occur in any of the following cases. |
- | When the specified section-name, file, or module cannot be found |
- | When section-name is not specified |
- | A warning will be output and this option ignored in the following case. |
- | When the -nooptimize option is specified |
[Example of use]
- | To suppress link-time optimization of the .SEC1 section, describe as: |
>rlink a.obj b.obj -optimize -section_forbid=(.SEC1)
|
- | To suppress link-time optimization of the .SEC1 and .SEC2 sections in a.obj, describe as: |
>rlink a.obj b.obj -optimize -section_forbid=a.obj(.SEC1,.SEC2)
|