When the -show=symbol option is specified, the external defined symbol or static internal defined symbol address, size, type, and whether optimization is applied are output in the order of address.
When the -show=reference option is specified, the reference count of each symbol is also output.
The output example of the symbol information is shown below.
*** Symbol List ***
SECTION=(1)
FILE=(2)
(3) (4) (5)
START END SIZE
(6) (7) (8) (9) (10) (11)
SYMBOL ADDR SIZE INFO COUNTS OPT
SECTION=.text
FILE=sample.obj
00000000 00000023 24
_main
00000000 0 func ,g 0
_func_01
00000018 0 func ,g 0
SECTION=.bss
FILE=sample.obj
fe600004 fe60000b 8
_gvall
fe600004 4 data ,g 0
|
|
|
|
|
|
Section name
The name of the section is output.
|
|
|
File name
The file name is output.
|
|
|
Start address
The start address of the corresponding section included in the file shown in (2) is output.
This is expressed in a hexadecimal number.
|
|
|
End address
The end address of the corresponding section included in the file shown in (2) is output.
This is expressed in a hexadecimal number.
|
|
|
Section size
The size of the corresponding section included in the file shown in (2) is output (in byte units).
This is expressed in a hexadecimal number.
|
|
|
Symbol name
The symbol name is output.
|
|
|
Symbol address
The symbol address is output.
This is expressed in a hexadecimal number.
|
|
|
Symbol size
The symbol size is output (in byte units).
This is expressed in a hexadecimal number.
|
|
|
Symbol type
The data type and declaration type are output.
func: Function name
data: Variable name
entry: Entry function name
none: Undefined (label, assembler symbol)
g: External definition
w: Weak definition
l: Internal definition
|
|
|
Reference count of symbol
The reference count of the symbol is output.
This is expressed in a hexadecimal number.
This item is output only when the -show=reference option is specified.
When the reference count of the symbol is not output, "*" is output.
|
|
|
Whether optimization is applied
Whether optimization is applied is output.
ch: Symbol changed by optimization
cr: Symbol generated by optimization
mv: Symbol moved by optimization
|
When the -show=struct option is specified, the information regarding the structure and union members defined in the files that have been compiled with -g specified is also output. An output example of the structure member information is shown below.
*** Symbol List ***
SECTION=(1)
FILE=(2) START END SIZE
(3) (4) (5)
SYMBOL ADDR SIZE INFO COUNTS OPT
(6) (7) (8) (9) (10) (11)
STRUCT SIZE
(12) (13)
MEMBER ADDR SIZE INFO
(14) (15) (16) (17)
SECTION=.bss
FILE=C:¥Users¥b1501079¥Desktop¥a.obj
00001000 00001007 8
_st
00001000 8 data ,g 0
struct {
8
_st.mem1
00001000 4 int
_st.mem2
00001004 2 short
_st.stmem
00001006 2
struct {
2
_st.stmem.mem3
00001006 1 char
_st.stmem.mem4
00001007 1 char
}
}
|
|
|
|
|
|
struct is output for a structure or union is output for a union.
|
|
|
Total size of the structure or union
|
|
|
The member name is concatenated after a symbol name with a dot (.).
|
|
|
The member address is output.
|
|
|
The member size is output.
|
|
|
The member type is output.
|