Everything

+


Addition of values of first and second terms.

[Function]

Returns the sum of the values of the 1st and 2nd terms of an expression.

[Application example]

        .org    0x100
START:  jr      START + 6       ; (1)

(1)

The jr instruction causes a jump to "address assigned to START plus 6", namely, to address "0x100 + 0x6 = 0x106" when START label is 0x100.