Everything

HIGH


Returns the high-order 8-bit value of a term.

[Function]

Returns the high-order 8-bit value of a term.

[Application example]

mov     HIGH(0xC08), r10       ; (1)

(1)

By executing a mov instruction, this operator returns the high-order 8-bit value "0xC" of the expression "0xC08".
Therefore, (1) in the above example can also be described as: mov 0xC, r10.