Everything
5.1.12 Identifiers

An identifier is a name used for symbols, labels, macros etc.

Identifiers are described according to the following basic rules.

-

Identifiers consist of alphanumeric characters and symbols that are used as characters (@,_, ., $)
However, the first character cannot be a number (0 to 9) or $.

-

Reserved words cannot be used as identifiers.
With regard to reserved words, see "5.5 Reserved Words".

-

The assembler distinguishes between uppercase and lowercase.