This option specifies the language standard of C source files and C++ source files.
[Specification format]
-lang={c|c99} [V1.11 or earlier]
-lang={c|c99|cpp14} [V1.12 or later]
|
- | Interpretation when omitted |
Compilation is executed in accord with the C90 standard.
[Detailed description]
This option specifies the language standard of the source file.
- | When the -lang=c option is specified or the option is omitted, compilation is executed in accord with the C90 standard. |
- | When the -lang=c99 option is specified, compilation is executed in accord with the C99 standard. |
- | When the -lang=cpp14 option is specified, compilation is executed in accord with the C++14 standard. [V1.12 or later] |
- | If any option other than -lang=c, -lang=c99, or -lang=cpp14 is specified, an error occurs. |
[Remark]
- | If a C source file is specified for input when the -lang=cpp14 option is specified, a compile error occurs.
[V1.12 or later] |
- | This compiler does not support the following language standards. |
- | Some header files and standard library functions in the C90/C99 language standard |
- | Complex number types in the C99 language standard |
- | Variable-length arrays in the C99 language standard |