Everything

 

-asmopt


This option specifies assemble options.

[Specification format]

-asmopt=arg

 

-

Interpretation when omitted

Only the assemble options specified by the compilation driver are passed to the assembler.

[Detailed description]

-

This option passes arg to the assembler as the assemble option.

-

An error will occur if arg is omitted.

[Example of use]

-

To pass the -prn_path option to the assembler, describe as:

>ccrl -c -asmopt=-prn_path -cpu=S2 -dev=dr5f100pj.dvf main.c

 

The -asmopt option specified in the above example has the same effect as the following example.

>ccrl -S -cpu=S2 -dev=dr5f100pj.dvf main.c
>asrl -prn_path -cpu=S2 -dev=dr5f100pj.dvf main.asm