This option specifies the device file that the assembler and optimizing linker use.
[Specification format]
- | Interpretation when omitted |
No device file is passed to the assembler or optimizing linker.
[Detailed description]
- | This option specifies device file file that the assembler and optimizing linker use. |
- | If this option is omitted at compilation, an error may occur in the assembler or the optimizing linker. |
- | An error will occur if file is omitted. |
[Example of use]
- | To specify device file "DR5F100PJ.DVF" that the assembler and optimizing linker use, describe as: |
>ccrl -cpu=S2 -dev=dr5f100pj.dvf main.c
|