This option displays the version information of asrl.
[Specification format]
- | Interpretation when omitted |
Assembling is performed without displaying the version information of asrl.
[Detailed description]
This option outputs the version information of asrl to the standard error output.
It does not execute assembling.
[Example of use]
- | To output the version information of asrl to the standard error output, describe as: |