This option outputs the specified warning message.
[Specification format]
-warning={num|num1-num2}[, ...]
 | 
 
 
-  | Interpretation when omitted  | 
 
All warning messages are output.
[Detailed description]
-  | This option outputs the specified warning message.  | 
 
-  | Specify the error numbers as num, num1, and num2. 
If the error number that does not exist, it will be ignored.  | 
 
-  | An error will occur if num, num1, or num2 is omitted.  | 
 
-  | If num1-num2 is specified, it is assumed that error numbers within the range have been specified.  | 
 
-  | The error number specified by this option is the rightmost 5 digits of the 7-digit number following the "W".  | 
 
-  | This option can only control output for warning messages with message numbers (here written with the component number) in the range from 0550000 to 0559999.  | 
 
[Example of use]
-  | To output warning message "W0550001" and "W0550005", describe as:  | 
 
>asrl -waning=50001,50005 -dev=dr5f100pj.dvf main.asm 
 |