This option specifies the execution start address.
This option defines execution start address with external defined symbol symbol or address address. |
Specify address in hexadecimal. |
If the specified symbol name is a C variable name, add "_" at the head of the definition name in the program. |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |
Be sure to specify symbol if you intend to enable inter-module optimization (-optimize[={symbol_delete|speed}]). If address is specified with this option, optimization regarding deletion of unreferenced symbols will be disabled. |
If the address specified by the -entry option is included in any of the sections allocated by the -start option, optimization in the range from the first address of the section up to the address specified by the -entry option will be suppressed. |