This option replaces library modules.
[Specification format]
-REPlace=suboption[, ...]
suboption := {file|file(module[, ...])}
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option replaces specified file file or library module module with the module having the same name in the library file specified by the -library option. |
[Example of use]
- | To replace file1.obj with module "file1" in library file lib1.lib, describe as: |
>rlink -library=lib1.lib -replace=file1.obj -form=library
|
- | To replace module "mdl1" with module "mdl1" in library file lib1.lib, describe as: |
>rlink -library=lib2.lib -replace=lib1.lib(mdl1) -form=library
|
[Remark]
- | If the -form={object|relocate|absolute|hexadecimal|stype|binary} option and the -extract or -strip option is specified, this option will be invalid. |
- | Operation is not guaranteed if this option is used in combination with compile option -Omerge_files. |