This option specifies the output file.
[Specification format]
- | Interpretation when omitted |
A standard library with the file name stdlib.lib is generated in the current folder.
[Detailed description]
- | This option specifies the output file name for the standard library. |
- | file should be specified by using an absolute path or a relative path. |
- | A relative path used to specify file is interpreted as the relative path from the current folder. |
- | An error will occur if file is omitted. |