This option controls the copyright display.
[Specification format]
- | Interpretation when omitted |
The copyright is displayed.
[Detailed description]
- | When -logo is specified, the copyright is displayed. When -nologo is specified, the copyright is not displayed. |
- | If these options are specified at the same time, the option specified last will be valid. |