Everything
3.7 Variable/Function Information File

This section explains the variable/function information file.

The variable/function information file is in the text format and contains declarations of the saddr variable or callt function for variables and functions defined in the C source file.