Addition of values of first and second terms.
[Function]
Returns the sum of the values of the 1st and 2nd terms of an expression.
[Application example]
START: BR !!START + 6 ; (1)
|
(1) | The BR instruction causes a jump to "address assigned to START plus 6", namely, to address "0x100 + 0x6 = 0x106" when START label is 0x100. |