5.1.10
2-byte separation operators
The following 2-byte separation operators are available.
|
|
HIGHW
|
Returns the high-order 16-bit value of a term
|
LOWW
|
Returns the low-order 16-bit value of a term
|
MIRHW
|
Obtains the higher-order 16 bits of the corresponding address in the mirror destination area when the value of the specified term is in the mirror source area
|
MIRLW
|
Obtains the lower-order 16 bits of the corresponding address in the mirror destination area when the value of the specified term is in the mirror source area
|
SMRLW
|
Adds an offset to the mirror destination to the address of a symbol, adds an integer value to the obtained value, and then obtains the value of the lower-order 16 bits among the 32-bit value of the result
|