Returns the size of the term section after linking.
Returns the size of the term section after linking.
Allocates a 4-byte area, and initializes it with the size of the default section (.text).
To allocate a 4-byte area and initialize it with the size of the user-defined section (user_text).
To use this operator in conjunction with STARTOF:
To specify EX_ATF2000 as the name for an absolute section.
This operator can be specified in combination with SIZEOF by using the binary operator "+". |