Defines the amount of stack usage for a symbol.
[Syntax]
Symbol field
|
Mnemonic field
|
Operand field
|
Comment field
|
|
.STACK
|
symbol-name=absolute-expression
|
[; comment]
|
[Function]
- | The .STACK directive is compiler debugging information. |
[Description]
- | This defines the amount of stack usage for a symbol. |
- | The amount of stack usage for a symbol can only be defined once, and subsequent definitions are ignored. |
- | The amount of stack usage can only be a multiple of 2 within the range of 0x0000 to 0xFFFE. |
- | The information handled by the .STACK directive is the function information of the C source program that the compiler outputs. |