Everything
5.3.3 Mirror source area reference control instructions

Using the mirror source area reference control instruction enables reference to external reference names in the sections allocated at mirror source area addresses.

The following mirror source area reference control instructions are available.

Table 5.27

Mirror Source Area Reference Control Instructions

Control Instruction

Overview

MIRROR

Declares that an external reference name is allocated to the mirror source area