Everything
6. SECTION SPECIFICATIONS

In an embedded application such as allocating program code from certain address or allocating by division, it is necessary to pay attention in the memory allocation.

To implement the memory allocation as expected, program code or data allocation information should be specified in optimizing linker.

Sections which are units for memory allocation are described in this chapter.