Conversion of character string to floating-point number (double type)
double __far atof(const char __near *nptr);
double __far _COM_atof_f(const char __far *nptr);
If the partial character string has been converted, the resultant value is returned. If the character string could not be converted, 0 is returned.
If an overflow occurs, atof returns ±∞ and sets macro ERANGE to global variable errno.
If an underflow occurs, atof returns 0 and sets macro ERANGE to global variable errno.
This function converts the first portion of the character string indicated by nptr into a float type representation.