Everything
8.1 Outline

The startup processing is used to initialize a section for embedding the user application described with the C language to the system or start the main function.

In order to execute a created program, a startup routine appropriate for that program has to be created.