-
If the number of digits of floating-point numbers is high in printf, sprintf, vprintf, vsprintf, scanf, sscanf, atof, atoff, strtod, or strtof, the error is enlarged.
If the absolute value of an exponential is high in pow, the error is enlarged.