< Optimizing Linkage Editor (rlink) Options / Output Options >
When the entry point address is larger than the specified address field, select the type of end record that suits the address of the entry point.  | 
When this option is omitted, the end record that is output will suit the address of the entry point.  | 
An S-type end record that is interpreted as a 32-bit address (S7) is output regardless of the address range.  | 
When -form={stype} is not also specified, an error message is output in response to this option and execution is terminated.  |