Be sure to append a colon (:) to the end of a label.
Defining a symbol name which is the same as that of an existing section is not possible. If a section and symbol with the same name are defined, the section name will be effective, but the symbol name will lead to an E0552118 error.